Min_Profile_Velocity

Index.Sub 2010.0H
Data Type Unsigned16
Access Read/Write
PDO Mappable No
Unit User-defined velocity unit (1)

Range

0 to ‘Max’ (2)
Default Value 250
Store Supported No
Description

This object defines the minimum motor velocity for the acceleration and deceleration ramp.

 It can only be set with the motor at a standstill and cannot be higher than the Max_Profile_Velocity object. If the value to be set is lower than the minimum value of range, the minimum value is stored.

 If the value to be set is higher than the maximum value of range, the maximum value is stored.

Notes

(1) See Factor Group

(2) ‘Max’  value is calculated according to this formula :

 Max(User-defined velocity unit) = 150000 * (2013.2H / 2013.1H) * (60EF.0H / 65536)

Objects in 'Max' value formula:

2013.2H vl Dimension Factor (denominator)
2013.1H vl Dimension Factor (numerator)
60EF.0H Motor_Resolution
  • This object is not available in EtherCAT fieldbus.